CIMPLICITY REST API Web Service
CIMPLICITY REST API Web Service / CimDerivedPoint Json Schema
CimDerivedPoint Json Schema
Description
Contains the properties pertaining to Derived Point Configuration
Overview
CimDerivedPoint
Contains the properties pertaining to Derived Point Configuration
CalculationType : CimPointCalcTypesEnum
Specifies calculation types of points
InitState : CimDpInitStateEnum
Specifies initial value for a global or derived point.
InitValue : string
is string containing the initial value for the point.
Local : boolean
is boolean indicating if the point is local. Local points can be used to hold intermediate values of expressions. The value of local points are not available to applications, they are only used internally by the derived point process to perform calculations.
PointExpression : string
is string containing the expression for the point.
PointSetInterval : string
is string containing the interval to update the timer counter point. The format is HH:MM:SS using a 24 hour clock.
PointSetTime : string
is string containing the start time for the timer counter point. The format is HH:MM:SS using a 24 hour clock
ProcessID : string
is a string specifying the derived point process supporting this point. Normally this will be 'SPM' or '_PTDP_RP'. This must identify a valid derived point processor process ID. It should not be changed unless you are using structure point processing
ResetPointID : string
is a string containing the name of the reset point.
RolloverVal : integer
is a long integer defining the roll over value for delta accumulator function.
VarianceValue : integer
is long integer defining the maximum variance value to be used for delta accumulator functions.
Properties
NameDescriptionData Type
Specifies calculation types of pointsCimPointCalcTypesEnum
Specifies initial value for a global or derived point.CimDpInitStateEnum
is string containing the initial value for the point.string
is boolean indicating if the point is local. Local points can be used to hold intermediate values of expressions. The value of local points are not available to applications, they are only used internally by the derived point process to perform calculations.boolean
is string containing the expression for the point.string
is string containing the interval to update the timer counter point. The format is HH:MM:SS using a 24 hour clock.string
is string containing the start time for the timer counter point. The format is HH:MM:SS using a 24 hour clockstring
is a string specifying the derived point process supporting this point. Normally this will be 'SPM' or '_PTDP_RP'. This must identify a valid derived point processor process ID. It should not be changed unless you are using structure point processingstring
is a string containing the name of the reset point.string
is a long integer defining the roll over value for delta accumulator function.integer
is long integer defining the maximum variance value to be used for delta accumulator functions.integer
See Also